MCU with  Hbridge drive(DC Motor)+Can Module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU with  Hbridge drive(DC Motor)+Can Module

Jump to solution
2,683 Views
mithunp_s
Contributor III

Hi All,

One of my customer is looking for MCU with  Hbridge drive(DC Motor)+Can Module feature, we got this MICU "MM912G634DM1AE" but this has no CAn, please someone suggest a MCU with both features if not available please suggest other option.


This is for Temperature control Application. Attached file for your reference with MCU specs.


Thanks in Advance


Regards

Mithun


Labels (1)
0 Kudos
Reply
1 Solution
2,530 Views
RadekS
NXP Employee
NXP Employee

I would like to recommend S12ZVM family:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12ZVM

This is also suitable for driving BLDC and PMSM motors.

If you would like get something more “conservative”, I would like to recommend for example S12G family:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12G


View solution in original post

0 Kudos
Reply
1 Reply
2,531 Views
RadekS
NXP Employee
NXP Employee

I would like to recommend S12ZVM family:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12ZVM

This is also suitable for driving BLDC and PMSM motors.

If you would like get something more “conservative”, I would like to recommend for example S12G family:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12G


0 Kudos
Reply