MCU with  Hbridge drive(DC Motor)+Can Module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU with  Hbridge drive(DC Motor)+Can Module

ソリューションへジャンプ
2,681件の閲覧回数
mithunp_s
Contributor III

Hi All,

One of my customer is looking for MCU with  Hbridge drive(DC Motor)+Can Module feature, we got this MICU "MM912G634DM1AE" but this has no CAn, please someone suggest a MCU with both features if not available please suggest other option.


This is for Temperature control Application. Attached file for your reference with MCU specs.


Thanks in Advance


Regards

Mithun


ラベル(1)
0 件の賞賛
返信
1 解決策
2,528件の閲覧回数
RadekS
NXP Employee
NXP Employee

I would like to recommend S12ZVM family:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12ZVM

This is also suitable for driving BLDC and PMSM motors.

If you would like get something more “conservative”, I would like to recommend for example S12G family:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12G


元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,529件の閲覧回数
RadekS
NXP Employee
NXP Employee

I would like to recommend S12ZVM family:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12ZVM

This is also suitable for driving BLDC and PMSM motors.

If you would like get something more “conservative”, I would like to recommend for example S12G family:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12G


0 件の賞賛
返信