MCU Flasher for MM9z1_638

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU Flasher for MM9z1_638

Jump to solution
1,705 Views
Boris_Bloxsberg
Contributor III

Hi,


I want to implement an own software applicantion to flash the MM9z1_638. Could somebody recommand a device to flash this type of MCU and this type of usecase?



Thanks.

0 Kudos
Reply
1 Solution
1,669 Views
danielmartynek
NXP TechSupport
NXP TechSupport

There is no such list.

PEMicro programmers are recommended on each NXP S12Z MCU website though.

S12ZVM:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-m...

 

BR, Daniel

View solution in original post

3 Replies
1,681 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Boris_Bloxsberg,

Do you mean a debugger/programmer?

Since the MM9Z1_638 has the S12Z core, you can use those that support S12Z (MagniV).

For example PE Micro Multilink:

https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&productTab=3

danielmartynek_0-1689148077888.png

 

Regards,

Daniel

1,676 Views
Boris_Bloxsberg
Contributor III

Thanks @danielmartynek  for the reply.

Yes, I need a programmer. Is there a list aviable with supported programmers for the S12Z? 

Regards,

 

0 Kudos
Reply
1,670 Views
danielmartynek
NXP TechSupport
NXP TechSupport

There is no such list.

PEMicro programmers are recommended on each NXP S12Z MCU website though.

S12ZVM:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-m...

 

BR, Daniel