MC33812 / S12P Small Engine Control.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33812 / S12P Small Engine Control.

2,190件の閲覧回数
francescodisilv
Contributor I

hi, I bought the kit reference design - MC33812 / S12P Small Engine Control. I wanted to ask if the sample software in the CD is ready to use or you need to change. The simulation runs with debugging, but there are no signs of spark and fuel injection. In addition, the routines spi, sci and mc33812perchè they are not prepared for the micro mc9s12p? thanks for any clarification

ラベル(1)
0 件の賞賛
返信
1 返信

1,979件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi Franceso,

The SW included in the CD is ready to use. It is already configured for S12P. You can fidn the rouines in the Low_Level subfolder which is Sources folder of the SW Example project.

Here are some links to smilar topics on the community that can be of help:

Re: Help, NEW to Codewarrior IDE S12 V5.0 and KIT33812ECUEVME
Re: KIT33812ECUEVME

Regards,

iggi

0 件の賞賛
返信