Leaving input capture pin floating when not in use

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Leaving input capture pin floating when not in use

1,824 次查看
gator
Contributor I

I'm wondering if there are any negative consequences of having an input capture pin floating as long as the input capture interrupt is not enabled. I won't be using the pin when it's in this state, I'm just wondering if this could cause problems.

Thanks

0 项奖励
回复
3 回复数

1,533 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

the same considerations. Probably slide 24 add some info. ... setting internal pull up requires no additional HW and it solves your issues.

Best regards,

Ladislav

0 项奖励
回复

1,533 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

No there i no problem if you use it in the IC mode as well as in the OC mode when no action is selected or when selected action will not affect anything. The input logic behaves on the basis of the TCTL3/4 registers setup.  Read TCTL3/4 registers and TCTL1/2 registers. I can't see MCU number to be more specific but it is common feature.... you can disable capture in IC mode and action on output pin in OC mode.

Plus, please read more info for

http://www.nxp.com/docs/en/application-note/AN5207.pdf 

and

http://www.nxp.com/docs/en/application-note/AN3262.pdf 

search for "unused" keyword.

If this does not answer your question(s), or I have forgotten something, or if you need more assistance, please contact me again.

Best Regards, Ladislav

0 项奖励
回复

1,533 次查看
gator
Contributor I

Sorry, I forgot to mention the MCU we are working with is the MC9S12DP512. Does that change anything?

Thank you

0 项奖励
回复