LIN pin capicitance on S12ZVL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LIN pin capicitance on S12ZVL

2,864 次查看
rajivbandodkar
Contributor II

Refer to the speck on LIN Phy in electrical section of S12ZVL reference manual. There are two specks: 

1. Maximum capacitance allowed on slave node including external components   Nominal    220 pF

                                                                                                                                    Max         250 pF

2.Capacitance of the LIN pin, Recessive state                                                         Nominal    20 pF

                                                                                                                                    Max         45 pF

 

There is a confusion weather 220pF can be used as 220+45 = 265 pF. This value is more than 250pF allowed...

 

Please clarify...

 

Regards,

Rajiv Bandodkar.

标签 (1)
0 项奖励
回复
2 回复数

2,660 次查看
rajivbandodkar
Contributor II

Thanks, clear,

Regards

Rajiv Bandodkar.

0 项奖励
回复

2,660 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi

The capacitance of the slave node defines the total node capacitance at the connector of the slave unit including the physical bus driver (Transceiver) and all other components applied to the LIN bus pin like capacitors or protection circuitry.

In other words, C_slave (250pF) is maximal capacitance of the slave node, which includes capacitance of the LIN pin (45pF max) and the rest (205pF) is left for a protection circuitry etc.  

Regards

Daniel

0 项奖励
回复