KIT33812ECUEVME

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,797件の閲覧回数
domenicocaliend
Contributor I

Hello Everybody

 

Has anyone have tried to use this kit with a TWO CYLINDER / 4 STROKE engine?

 

I would like just to exchange views and solutions.

 

Thank you.

Regards.

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,543件の閲覧回数
iggi
NXP Employee
NXP Employee

The KIT33812ECUEVME uses our MC33812 chip, which is intended for “Single or Dual” Cylinder  (4 Stroke or 2 stroke) engines.  It drives two Injectors independently, but drives only “One” Coil. Hence, technically both Spark Plugs for the Dual Cylinders will fire at the same time, with one wasted spark. This chip does not have VRS on board.


The next version is our MC33813, which is similar to MC33812 but intended for “Single” Cylinder with VRS on-board.  Hence, reduces the need for an external VRS chip and technically reduces the size of the PCB.


Furthermore, we have MC33814, which is very much the same as MC33813. However, it supports up to TWO Cylinder (4 Stroke or 2 Stroke) with “independent” support for Two Injectors and Two Coil along with VRS on-board.


So, you could use either MC33812 or MC33814 depending on your specific needs. The datasheets are below:

http://cache.freescale.com/files/analog/doc/data_sheet/MC33812.pdf

http://cache.freescale.com/files/analog/doc/data_sheet/MC33814.pdf


Best Regards,

Ivan

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,544件の閲覧回数
iggi
NXP Employee
NXP Employee

The KIT33812ECUEVME uses our MC33812 chip, which is intended for “Single or Dual” Cylinder  (4 Stroke or 2 stroke) engines.  It drives two Injectors independently, but drives only “One” Coil. Hence, technically both Spark Plugs for the Dual Cylinders will fire at the same time, with one wasted spark. This chip does not have VRS on board.


The next version is our MC33813, which is similar to MC33812 but intended for “Single” Cylinder with VRS on-board.  Hence, reduces the need for an external VRS chip and technically reduces the size of the PCB.


Furthermore, we have MC33814, which is very much the same as MC33813. However, it supports up to TWO Cylinder (4 Stroke or 2 Stroke) with “independent” support for Two Injectors and Two Coil along with VRS on-board.


So, you could use either MC33812 or MC33814 depending on your specific needs. The datasheets are below:

http://cache.freescale.com/files/analog/doc/data_sheet/MC33812.pdf

http://cache.freescale.com/files/analog/doc/data_sheet/MC33814.pdf


Best Regards,

Ivan

0 件の賞賛
返信
2,543件の閲覧回数
domenicocaliend
Contributor I

Thank you, Ivan.

In case of a 4-stroke 2-cylinder engine, when the period is 720° long, how can the board distinguish if the engine is in "intake/compression" or in "power/exhaust" strokes without a cam-sensor?

Thank you again.

Regards.

2,543件の閲覧回数
iggi
NXP Employee
NXP Employee

FYI,


all of our Small Engine chips (MC33812, MC33813 and MC33814) have a MAP (Manifold Air Pressure) sensor input.  User can use that information to detect which cycle it is on.  That is the pressure would be different on intake/compression stroke versus power/exhaust stroke.  Hence, if taking advantage of that, then user would be able to avoid wasted spark.

Hope this helps.

0 件の賞賛
返信