Is there any shutdown procedure before COP reset?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any shutdown procedure before COP reset?

1,363 Views
lx
Contributor I

HI,

 

I am using S12DJ128. When COP reset, PCAN View captured a number of Stuff Erroe, Rx, and other Rx error while power reset did not. Is there any shutdown procedure for CAN module I shall do before COP reset?

 

Thanks

Labels (1)
0 Kudos
Reply
3 Replies

1,162 Views
kef
Specialist I

Do you trigger COP reset intentionally or is it some undesired unpexpected event? If 2nd, then you can only fix you FW, so that COP doesn't happen. When COP times out, it is too late to shut down MSCAN. Not only CPU, but also all peripherals including MSCAN are reset, so any ongoing transmission from your MCU may be abrupt cancelled in the middle of message, leading to some CAN errors.

You should make sure MCU CAN pins are pulled up and not floating when reset occurs.

0 Kudos
Reply

1,162 Views
lx
Contributor I

We trigger COP reset intentionally.

 

How to make sure MCU CAN pins are pulled up and not floating when reset occurs?

 

Thanks

0 Kudos
Reply

1,162 Views
kef
Specialist I

You could use oscilloscope.

Add pull up resistors.

I'm not sure, but maybe there's CAN transceiver on market with built in pull up devices on input pins?

What port pins is MSCAN routed to in your application? Port J has pull ups enabled out of reset, but not port M...

0 Kudos
Reply