Is it necessary to use PDO and PDOCLK for debugging and downloading the S912ZVML32F3MKH chip program

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it necessary to use PDO and PDOCLK for debugging and downloading the S912ZVML32F3MKH chip program

998 次查看
yankui666
Contributor III

I am using the S912ZVML32F3MKH chip. If I don't use the PDO and PDOCLK pins and only use BKCD, RST, GND, and VDDX, can I debug and download the program properly. Do PDO
and PDOCLK require a download port to debug the download program?

0 项奖励
回复
2 回复数

968 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

 

We recommend using all the necessary pins so that all debugging functions are available. You don't know if you'll ever need it and then you'll miss it. For example, the trace function. In addition, the debugger can have a property implemented when it needs these pins. We don't see it because it is given by the implementation of the debug interface, its protocol and properties, which is not our product. Of course, if you check your specific usage, then the possibility is there, but as I already wrote, it is better to use the full interface.

Best regards,

Ladislav

0 项奖励
回复

123 次查看
emilio
Contributor I
If I have the Multilink ans Codewarrior, how can I download the firmware?, any sample project or documentation related, how can I do?
I am try to use BKCD, RST, GND, and VDDX.
0 项奖励
回复