INPUT CAPTURE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,854件の閲覧回数
kaarthichandras
Contributor II

Hi,

Iam using S12zvml31 controller for sensorless commutation for bldc motor control. I configured TIM0 channel 0 and channel 3 as output compare mode for sensorless algorithm. Now I want to measure external pwm pulse through input capture, in which pin I have to connect that pwm signal. And how to use that TIM0?

Thanks and regards,

Kaarthi.

0 件の賞賛
返信
1 解決策
1,589件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

You can refer to S12ZVL-TIM-FrequencyMeasurement-V1_0-CW106-TIC-EXAMPLE 

It can be modified for pulse width measurements.

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,590件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

You can refer to S12ZVL-TIM-FrequencyMeasurement-V1_0-CW106-TIC-EXAMPLE 

It can be modified for pulse width measurements.

Regards,

Daniel

0 件の賞賛
返信