How to use Rappid bootloader with S12ZVML-MINIBRD kit ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use Rappid bootloader with S12ZVML-MINIBRD kit ?

1,852件の閲覧回数
Maciek
Contributor V

I've flashed S12ZVM.rbf file into the board. When I'm trying download my application using Rappid PC-side application - I get the following error message: 'CCP Communication Error. Loss Communicatin with CCP MCU. Please cycle power and try again." Of course cycling power doesn't help...
How to slove this problem ?
Does this (S12ZVM.rbf) Rappid bootloader work with UART1 (which is accessible via USB on this board) ?

Thanks
Maciek

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,581件の閲覧回数
fengwang
Contributor I

Hello Maciek,

How did you solved this error , I have the trouble like you ! Can you help me ?

many thanks

Regards,

Feng

0 件の賞賛
返信

1,581件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

here is a webpage that gives Overview of RAppID Bootloader. You can launch a live presentation video or just open a presentation document.

Overview of RAppID Bootloader|NXP 

Btw, please ensure the USB-to-SCI (UART port) operates correctly.

Check on your PC in Device and Printers if you see as below:

pastedImage_1.png

and Device Manager:

pastedImage_2.png

Hope this helps.

Regards,

iggi

 

0 件の賞賛
返信