How to use MACT to rotate the motor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use MACT to rotate the motor

656件の閲覧回数
fanlikang
Contributor II
Dear :

    Some problems occurred during the use of MACT, resulting in the motor not rotating I want to know where the problem is. The specific description of the problem is as follows:

1)When I used MACT to debug the motor, the development board reported the GDU fault.

fanlikang_0-1678761627229.png

 

2)This problem cannot be solved by using the fault clearing button in MACT. Because I reprogram PMFreeloadA_ In the ISR (void) function, a piece of code was imposed to solve the problem. Now GDU has no fault, but I don't know whether the code I wrote is appropriate?

fanlikang_1-1678761627454.png

 

3)When I connect to MACT again, there is no GDU fault, but FOC fault. I don't know what causes this fault, so I want to seek your help.

fanlikang_2-1678761627424.png

 

I want to seek help to get the correct use of MACT.

Best wishes

fanlikang

0 件の賞賛
返信
0 返答(返信)