hello
Is there a way to revert the application during bootloader operation on the HCS12X series chip?
example:
- Unexpected interruption during flash erase in bootloader
- The application operates normally after reset
- Assuming that the application is already loaded
I can't seem to find the code in AN4258.
解決済! 解決策の投稿を見る。
Hi,
I suggest to check CRC of the application before you jump into it to be sure it is OK.
In the case you want to use, go back, into the original application than it is necessary to split flash into 2 spaces and use A/B swap method where new apps is switched to after it is chceck and we still have possibility to go to the previous apps. The issue of this method is the size of the memory.
Best regards,
Ladislav
In the end, it seems like there is only a dual bank method.
thank you
Hi,
I suggest to check CRC of the application before you jump into it to be sure it is OK.
In the case you want to use, go back, into the original application than it is necessary to split flash into 2 spaces and use A/B swap method where new apps is switched to after it is chceck and we still have possibility to go to the previous apps. The issue of this method is the size of the memory.
Best regards,
Ladislav