How to reset MM9Z1-638 device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to reset MM9Z1-638 device

Jump to solution
2,333 Views
gumu
Contributor V

Hello,

I tried to use PCRReset() to reset MCU, it didn't work.

I'd like to know how to reset MM9Z1-638 device except watchdog?

Tags (1)
0 Kudos
Reply
1 Solution
2,242 Views
gumu
Contributor V

reset funcion is normal after removing 470nf capacitor .

View solution in original post

0 Kudos
Reply
4 Replies
2,243 Views
gumu
Contributor V

reset funcion is normal after removing 470nf capacitor .

0 Kudos
Reply
2,304 Views
gumu
Contributor V

Hi @Q_man ,

There is a 470nf capacitor between RESET and GND. Does it impact action of PCR_CTL.HWR(M)?

RESET and RESET_A is connected together.

0 Kudos
Reply
2,287 Views
Q_man
NXP Employee
NXP Employee

The 470nF is required to avoid the analog chip watchdog to periodically reset the uC. It should only be use for FLASH programming and should NOT be present in the application or software testing.

reset1.png

reset2.png

0 Kudos
Reply
2,315 Views
Q_man
NXP Employee
NXP Employee

Hi,

using the PCR_CTL.HWR(M) should generate a Reset (RESET_A should be pulled low) if the D2D Interface is initialized.

What hardware do you use?

- are the RESET_A and RESET pins connected?

- is there anything else connected externally to the RESET?

- is the D2D interface setup correctly? E.g. can you read from the analog die (e.g. the PCR_SR)

Rgds

W.

 

0 Kudos
Reply