How to reset MM9Z1-638 device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to reset MM9Z1-638 device

ソリューションへジャンプ
3,467件の閲覧回数
gumu
Contributor V

Hello,

I tried to use PCRReset() to reset MCU, it didn't work.

I'd like to know how to reset MM9Z1-638 device except watchdog?

タグ(1)
0 件の賞賛
返信
1 解決策
3,376件の閲覧回数
gumu
Contributor V

reset funcion is normal after removing 470nf capacitor .

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,377件の閲覧回数
gumu
Contributor V

reset funcion is normal after removing 470nf capacitor .

0 件の賞賛
返信
3,438件の閲覧回数
gumu
Contributor V

Hi @Q_man ,

There is a 470nf capacitor between RESET and GND. Does it impact action of PCR_CTL.HWR(M)?

RESET and RESET_A is connected together.

0 件の賞賛
返信
3,421件の閲覧回数
Q_man
NXP Employee
NXP Employee

The 470nF is required to avoid the analog chip watchdog to periodically reset the uC. It should only be use for FLASH programming and should NOT be present in the application or software testing.

reset1.png

 

reset2.png

 

0 件の賞賛
返信
3,449件の閲覧回数
Q_man
NXP Employee
NXP Employee

Hi,

using the PCR_CTL.HWR(M) should generate a Reset (RESET_A should be pulled low) if the D2D Interface is initialized.

What hardware do you use?

- are the RESET_A and RESET pins connected?

- is there anything else connected externally to the RESET?

- is the D2D interface setup correctly? E.g. can you read from the analog die (e.g. the PCR_SR)

Rgds

W.

 

0 件の賞賛
返信