How to reduce quiescent current in STOP mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to reduce quiescent current in STOP mode

1,703 次查看
krishnakarthik6
Contributor II

Hi,

I am using mm9Z1_638 controller, I have enabled current measurement in the STOP mode by doing so i am observing the current consumption as 1.6mA. The total current consumed during STOP mode is calculated (or measured) using register ACQ_AHC after wake-up. I tried to reduce the current consumption by lowering the current measurement period by using the register ACQ_TCMP. The register ACQ_TCMP is set to 500msec, so current measurement is triggered at 500msec, but the ACQ_AHC is NOT sync in this case. I mean when ACQ_TCMP is 0 and my load current is 10mAmps, then after 60 sec stop i am observing ACQ_AHC as 600 mAmps which is correct, but when ACQ_TCMP is set to 500msec (0x1F4) i am observing the ACQ_AHC  as random value after wake-up. 

Please help me in resolving this. Thanks in advance

1 回复

1,486 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
As I was notified, you already discuss this topic directly with responsible application engineer.

Regards,
Daniel

0 项奖励
回复