How to measure the frequency?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to measure the frequency?

1,584件の閲覧回数
aaronlee
Contributor V

Hi,

We are using S12ZVCA(LQFP-48) and CodeWarrior 11.0 for measure the frequency of external signal. The frequency is between 1Hz and 500Hz.

Which pin do you recommend to connect the external signal?

Do you have example code?

Best Regards,

Aaron

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,462件の閲覧回数
aaronlee
Contributor V

Dear Daniel,

Thanks for your reply. We are design the schematic for PCB as following:

The PT4 & PT7 for frequency input. Do you have any recommend?

pastedImage_3.png

Best regards,

Aaron

0 件の賞賛
返信

1,462件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Aaron,

This is application-dependent, there is no recommendation,

BR, Daniel

0 件の賞賛
返信

1,462件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Please refer to this example:

https://community.nxp.com/docs/DOC-332554 

Thanks,

BR, Daniel

0 件の賞賛
返信