How to interface a display 240 x 64 with T6963 using MC9s12xdp512?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to interface a display 240 x 64 with T6963 using MC9s12xdp512?

1,477件の閲覧回数
sergioloncan
Contributor I

Need to develop a project with a display 240 x 64 (T6963) and I use MC9s12XDP512.

Is there any library to control?

Thank you.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,252件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

You can use any free port on the MCU, for example Port B, to connect 8x data lines D0-D7. Then you would need another port to connect control lines such as chip enable, R/W select etc.

Anyway, here is an older post which should be of interest. Please, check all the links, especially the one in the last response.

LCD Lib for MC9S08dz60 and T6963c

Regards,

iggi

0 件の賞賛
返信