How to interface a display 240 x 64 with T6963 using MC9s12xdp512?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to interface a display 240 x 64 with T6963 using MC9s12xdp512?

1,917 次查看
sergioloncan
Contributor I

Need to develop a project with a display 240 x 64 (T6963) and I use MC9s12XDP512.

Is there any library to control?

Thank you.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,692 次查看
iggi
NXP Employee
NXP Employee

Hi,

You can use any free port on the MCU, for example Port B, to connect 8x data lines D0-D7. Then you would need another port to connect control lines such as chip enable, R/W select etc.

Anyway, here is an older post which should be of interest. Please, check all the links, especially the one in the last response.

LCD Lib for MC9S08dz60 and T6963c

Regards,

iggi

0 项奖励
回复