How to add external ram in Processor Expert cpu build options

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to add external ram in Processor Expert cpu build options

1,781 次查看
AndersJ
Contributor IV
I want to add 256KB of external SRAM in normal expanded mode.
I am unable to add an external ram memory segment
using PE on the build options tab of the MC912SXD cpu bean.
* Name: RAM_External
* Qualifier: READ/WRITE
* Address: 140000 H
* Size 40000 H
 
At compile/link I get INTERNAL ERROR: at line 35 Unexpected status...... file: Drivers\HCS12\MC9S12_Linker.prg
 
Can anyone point out my error?
 
Thanks,
AJ
 
 
 
 
 
标签 (1)
0 项奖励
回复
1 回复

743 次查看
ProcessorExpert
Senior Contributor III

This problem has been fixed in Processor Expert v2.99 for CodeWarrior v4.7. This version of Processor Expert is available as a service Pack on Freescale web.

best regards
Vojtech Filip
Processor Expert Support Team
UNIS
0 项奖励
回复