How to add CAN controllers to a HCS12 based design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add CAN controllers to a HCS12 based design

1,873 Views
AndersJ
Contributor IV
What is the best way to add more CAN controllers to a HCS12 based design
when more controllers are needed than those available onboard the cpu?
 
Thanks,
Anders J
 
Labels (1)
0 Kudos
Reply
1 Reply

1,041 Views
Lundin
Senior Contributor IV
The best way is to change to a HCS12 with more MSCAN ports. If you need more than 5 CAN ports, well... then I suppose you could put additional controllers on the SCI. But before doing that, I would stop and seriously ask myself what I'm doing with so many CAN ports.
0 Kudos
Reply