How to Increase fifo bytes in S12ZVML12 CAN UDS Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Increase fifo bytes in S12ZVML12 CAN UDS Bootloader

1,317件の閲覧回数
MaxC00
Contributor I

while the application is set to receive in transfer data a block of 128 bytes, is it possible increase up to 1024 byte.  

I do this modifications but does not works:

#define TOTAL_FIFO_BYTES (4000u) (was 800u)

#define RX_TP_QUEUE_LEN (1050u) (was 150u)

Is it necessary change some other define?? or is not possible.

Thanks

0 件の賞賛
返信
2 返答(返信)

1,284件の閲覧回数
nxf10035
NXP Employee
NXP Employee

Hi,

    Default bootloader have 4 FIFO channels for transfer data as: Driver --> TP, TP-->UDS, UDS --> TP and TP --> driver. If increase the max received message length, should increase the FIFO channel size driver -- > TP and TP --> UDS. In addition, should modify the max UDS store message length and fls module the max program size.

    Hope this can help you. 

Best regards!

0 件の賞賛
返信

1,256件の閲覧回数
MaxC00
Contributor I

Hi,

thank you for reply, I have tried to increase the FIFO channel size and now the block sent by CAN is received correctly.

Unfortunately the received data are not programmed in the Flash.

Following the code I saw the Flask_app is tuned for a 128 bytes bloks. The received length is cast to a uint8. I think it is necessary a deep review to increase the buffer size over 128 bytes.

Best regards!

0 件の賞賛
返信