How can i erase the rom of HSC12xDt microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i erase the rom of HSC12xDt microcontroller

Jump to solution
1,007 Views
luck
Contributor III

i am working with freescale microcontroller HSC12xDT  i want to reset or clear the EEPROM.

 

Now currently the firmware i m working on has  a application part and a boot loader part.

 

so i wanted to add a functionality to bootloader which will erase ,clear or reset the EEPROM of the controller .

 

so can anyone help me on this .

Thnaks

Labels (1)
0 Kudos
Reply
1 Solution
908 Views
RadekS
NXP Employee
NXP Employee

In attachment you can find example codes for EEPROM at S12XDP512.

I hope that help you.


View solution in original post

0 Kudos
Reply
1 Reply
909 Views
RadekS
NXP Employee
NXP Employee

In attachment you can find example codes for EEPROM at S12XDP512.

I hope that help you.


0 Kudos
Reply