How can i erase the rom of HSC12xDt microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can i erase the rom of HSC12xDt microcontroller

ソリューションへジャンプ
991件の閲覧回数
luck
Contributor III

i am working with freescale microcontroller HSC12xDT  i want to reset or clear the EEPROM.

 

Now currently the firmware i m working on has  a application part and a boot loader part.

 

so i wanted to add a functionality to bootloader which will erase ,clear or reset the EEPROM of the controller .

 

so can anyone help me on this .

Thnaks

ラベル(1)
0 件の賞賛
返信
1 解決策
892件の閲覧回数
RadekS
NXP Employee
NXP Employee

In attachment you can find example codes for EEPROM at S12XDP512.

I hope that help you.


元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
893件の閲覧回数
RadekS
NXP Employee
NXP Employee

In attachment you can find example codes for EEPROM at S12XDP512.

I hope that help you.


0 件の賞賛
返信