How can i erase the rom of HSC12xDt microcontroller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can i erase the rom of HSC12xDt microcontroller

跳至解决方案
907 次查看
luck
Contributor III

i am working with freescale microcontroller HSC12xDT  i want to reset or clear the EEPROM.

 

Now currently the firmware i m working on has  a application part and a boot loader part.

 

so i wanted to add a functionality to bootloader which will erase ,clear or reset the EEPROM of the controller .

 

so can anyone help me on this .

Thnaks

标签 (1)
0 项奖励
回复
1 解答
808 次查看
RadekS
NXP Employee
NXP Employee

In attachment you can find example codes for EEPROM at S12XDP512.

I hope that help you.


在原帖中查看解决方案

0 项奖励
回复
1 回复
809 次查看
RadekS
NXP Employee
NXP Employee

In attachment you can find example codes for EEPROM at S12XDP512.

I hope that help you.


0 项奖励
回复