How can I program S12G without erasing data in EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I program S12G without erasing data in EEPROM

ソリューションへジャンプ
2,580件の閲覧回数
claudio_b
Contributor II

Hello eveybody,

 

How can I program S12G without erasing data in EEPROM. I think there is a setting in CW but I cannot find where.

 

Thank you in advance

ラベル(1)
0 件の賞賛
返信
1 解決策
2,417件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Claudio,

In CW debugger (hiwave.exe) menu – File – Configuration – Load tab – Advanced – mark EEPROM (blue background).

DFLASH.PNG

Note: Screenshot was captured for different MCU.

After next loading code, EEPROM programming will be skipped.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,418件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Claudio,

In CW debugger (hiwave.exe) menu – File – Configuration – Load tab – Advanced – mark EEPROM (blue background).

DFLASH.PNG

Note: Screenshot was captured for different MCU.

After next loading code, EEPROM programming will be skipped.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,417件の閲覧回数
kef2
Senior Contributor V

Don't have S12G at hand, but with minimal or none mods save/restore trick should work:

S12X flash memory copy

If not, try searching for flash save / restore and/or "AEFSKIPERASING" command.

0 件の賞賛
返信