External RAM Write and Read S12XE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External RAM Write and Read S12XE

2,249 Views
rayhall
Contributor V

I am using the S12XE and LY62W102516 1024K X 16 BIT LOW POWER CMOS SRAM.

 

When I write to the external SRAM and then read back the data, I do not get correct values.

 

Example of write and read.

24 24 24 24 24 24 24 24 24 24  // Write

00 20 24 24 24 24 24 24 24 24  // Read

 

This is the related code.

 

#define  WRITE_BYTE_B(a,d)  *((unsigned char *far)(a+0x200000UL))=d

#define  READ_BYTE_B(a)     *((unsigned char *far)(a+0x200000UL))

 

  uint8_t readStr[16];

 

  for(addr = 0; addr < 10; addr++) {         

     WRITE_BYTE_B(addr,0x24);  // write RAM address

  }

 

  for(addr = 0; addr < 10; addr++) {

    readStr[addr] = READ_BYTE_B(addr);  // read RAM address

  }

 

Ray.

Labels (1)
0 Kudos
Reply
1 Reply

1,841 Views
RadekS
NXP Employee
NXP Employee

Hi Ray,

Unfortunately I am not sure what could be reason for that behavior.

Problem could be in connection of address bits or some timing issue.

Please look at attached draft of document with external bus examples.

In case of MEBI module at S12XE, the data bus is always 16 bit. Please check how you connected A0 pin in SRAM memory.

Example code use MRAM with 35ns read and write cycle. Your SRAM may have 55 or 70ns read/write cycle. In that case some wait states may be necessary for fastest MCU bus clock (50MHz). See chapter 5.4.4 Stretched External Bus Accesses in RM for more details. You may also try temporarily decrease bus clock for testing whether it could be the root cause.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply