HW for programming LRAE into MC9S12C64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HW for programming LRAE into MC9S12C64

2,210件の閲覧回数
Joxalatorn
Contributor I

I can't get the LRAE programmed into the MC9S12C64 processor and just want to make sure what HW I need to do this.

I have this BDM http://www.m5k8.net/pl/hcs12/hcs12mem/

but it seems that it only can program a MCU that allready got the LRAE installed.

I have read a little about the TBDML but I can't figure out if it can program the LRAE.

 

What do I need to program the LRAE and how do I do it?

ラベル(1)
0 件の賞賛
返信
1 返信

1,067件の閲覧回数
DME
Contributor I

 

 I'm using the same podex  with hcs12mem tool. yesterday I programmed serial monitor bootloader into the same chip succesful. 

0 件の賞賛
返信