HC912B32 memory map

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,557件の閲覧回数
Yuping
Contributor I

Hi,

 

I am really a newbie...

I want to know what exactly are there in the memory. I could only find a very simple one like in the book "Software and Hardware Engineering" by Fredrick M. Cady. I want to have a detailed one which tells you what are the addresses for different interrupt vectors and control registers.

 

Btw, how could I load my program to the Flash memory?

 

Thanks!

 

Yuping 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,661件の閲覧回数
kef
Specialist I

If you are newbie, then why not start with current S12/S12X chips?

 

Vector table, register addresses, peripheral manuals all should be found in M68HC12B family datasheet:

 

http://www.freescale.com/files/microcontrollers/doc/data_sheet/M68HC12B.pdf

 

Also have a look at other documents:

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=68HC912B32&fpsp=1&tab=Documentation_T...

 

 

P&E USB-ML-12 + Codewarrior  should be enough for all current S08/RS08/S12/S12X/Coldfire_V1 chips. As far as I remember, old 912B32 requires also 12V programming voltage. In contrast to RS08, for which RevC and more recent USB-ML-12 can provide programming voltage via /RESET pin, which is available in standard BDM connector; B32 requires Vpp on some other pin. Good reason to start with more fresh chips!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,662件の閲覧回数
kef
Specialist I

If you are newbie, then why not start with current S12/S12X chips?

 

Vector table, register addresses, peripheral manuals all should be found in M68HC12B family datasheet:

 

http://www.freescale.com/files/microcontrollers/doc/data_sheet/M68HC12B.pdf

 

Also have a look at other documents:

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=68HC912B32&fpsp=1&tab=Documentation_T...

 

 

P&E USB-ML-12 + Codewarrior  should be enough for all current S08/RS08/S12/S12X/Coldfire_V1 chips. As far as I remember, old 912B32 requires also 12V programming voltage. In contrast to RS08, for which RevC and more recent USB-ML-12 can provide programming voltage via /RESET pin, which is available in standard BDM connector; B32 requires Vpp on some other pin. Good reason to start with more fresh chips!

0 件の賞賛
返信
1,661件の閲覧回数
Yuping
Contributor I

Hi Kef,

 

Thanks a lot for the information!! Seems I have a lot of work to do now. :smileyhappy:

X68HC912B32 is the only one available for me here. I did not know it's so old at first...

Anyway, I'll have to study more about it.

 

Thanks!

Yuping 

0 件の賞賛
返信