Grounding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Grounding

1,166件の閲覧回数
VP63
Contributor I

Hello,

I am using MCU S12ZVMC with external Xtal.

Should I connect VSS1 pin to the exposed pad and then Xtal local ground to pin VSS1?

Thanks in advance!

 

0 件の賞賛
返信
1 返信

1,156件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

The AN5207:

All GROUND pins of the microcontroller (VSSX1, VSSX2, VSS1, VSS2, VSSA, and VSSB, VSSC) must be connected together.

The reference manual:

1.7.4 Package and Pinouts

The following package options are offered.

  • 80LQFP-EP (exposed pad) with internal CANPHY and CAN VREG.
  • 64LQFP-EP (exposed pad) with internal LINPHY or HV physical interface.
  • 64LQFP-EP (exposed pad) with CAN VREG to support a low cost external CANPHY.
  • 48LQFP-EP (exposed pad)

The exposed pad must be connected to a grounded contact pad on the PCB.

The exposed pad has an electrical connection within the package to VSSFLAG (VSSX die connection).

The pin out details are shown in the following diagrams. Signals in brackets denote routing options.

 

Best regards,

Ladislav

0 件の賞賛
返信