Using CAN FD with S12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using CAN FD with S12

1,584件の閲覧回数
FenomenoKim
Contributor I

I am looking for a way to use CAN FD with S12. From what I’ve found, one method is to use an external CAN controller. Products like the TCAN4551 or MCP2518FD can be used in a configuration like MCU - SPI - Controller to utilize FD CAN.

What I’m curious about is whether NXP has a module like this, and if there’s an easier method than SPI control.

0 件の賞賛
返信
1 返信

1,546件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @FenomenoKim,

There is just one NXP Stand-alone CAN controller, but it does not support CAN-FD.

https://www.nxp.com/products/interfaces/can-transceivers/legacy-can/stand-alone-can-controller:SJA10...

As you mention, the solution is to use a 3rd-party controller with the S12 series.

There are S32K1xx, S32K3xx automotive MCUs that support CAN-FD though.

 

Regards,

Daniel

0 件の賞賛
返信