FlexRay Code Example for MC9S12XF512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexRay Code Example for MC9S12XF512

3,137 Views
pierrel
Contributor III

Hello,

 

I'm using the MC9S12XF512 microcontroller in order to develop a FlexRay application.

I already donwload the Node 1 and 2, FS and LS and StandAlone  code example. It is hard for me to understand how to use the differents functions.

My question is : Is there anybody who has already use one of the code examples for a FlexRay application and who has a main.c using functions for sent a FlexRay frame ?

I don't understand how to sent a frame with my own payload with all the functions.

 

Thank you,

Pierre

Labels (1)
2 Replies

2,736 Views
shanbh01
Contributor I

Dear Mr. Pierre Lebas,

Did you find someone who has already done this as its been two years since this post.

Could you help me  "How to send frames with my own payload" 

I could not find any help online.

I am new to this setup and i do not understand as well( doing this as part of my student project)

Thanks

0 Kudos
Reply

2,736 Views
iggi
NXP Employee
NXP Employee

Hi,

Certainly there is somebody, but it looks like none of them visit 16-bit community space.

I will see if there is a person who could join this thread and help you more with this.

Regards,

iggi

0 Kudos
Reply