over current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

over current

2,177件の閲覧回数
443115228
Contributor II

hello,

   Where do I go to modify the maximum current value, the maximum voltage value...

   why frac16(0.7)<frac16(0.68)?

0 件の賞賛
返信
3 返答(返信)

2,053件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

it is not clear what you are talking about. There is no additional what you use,......

Best regards,

Ladislav

0 件の賞賛
返信

2,053件の閲覧回数
443115228
Contributor II

Hi lama:

         I'm using 3-phase Sensorless Dual-Shunt PMSM S12ZVM Application – FOC driving example project.

         I_PH_OVER = 0.465*20?

         U_DCB_OVERVOLTAGE = 0.8*25?

         Both I_PH_OVER  and U_DCB_OVERVOLTAGE are defined as FRAC16(),  How do they know what to multiply by?

Actually,I changed the magnification on my own board,but I don't know how to modify the AD sample code

0 件の賞賛
返信

2,053件の閲覧回数
pachamatej
NXP Employee
NXP Employee

Hi,

you would need to use the MCAT control page (open the FreeMASTER project) and set the Imax on the Parameters tab as shown below. This parameter is not synced with the real-time app, so you need to click "Store Data" and then go to Output File tab and click "Generate Configuration File". Then you would need to rebuild your project in CodeWarrior and flash it. More info can be found in AN4642 or AN4912.

CurrentScale.png

If you would like to know more about 1.15 fixed point (frac16) calculation, please follow some books or internet resources. This is more generic topic than can be discussed/explained here.

I hope it helps,

Matej

0 件の賞賛
返信