Flash Programer for S12 series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Programer for S12 series

ソリューションへジャンプ
3,337件の閲覧回数
YANG-NMOG
Contributor I

Hello:

I am a engineer in the factory in China, we need to produce a new manufacture with use the MCU of S912ZVM.

For my job,I need to design a new automation-machine to do this. Could I get some advice of which Flash Programer can be used in my automation-machine?

I need to design a software to PC to  control the Flash Programer for the automation-chine.

So I need the Flash Progarmer have the API or SDK or other some thing to control

I think is U-MULTILINK-FX,but not sure.

Thank you !

0 件の賞賛
返信
1 解決策
3,325件の閲覧回数
ArchieLuo
Contributor III

可以使用Cyclone LC 或者 Cyclone FX,这两个工具是可以脱机烧录的,一般量产都会用这个工具。

U-MULTILINK-FX只是个调试器,必须连电脑使用。

可以使用PROGS12ZZ这个软件,搭配下载器使用。

如有疑问可以联系我~

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,309件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

Since we have no solution for mass production such as stand-alone programmers, you have to turn to third-party products.

I can confirm the information posted by lsssssssssss.

You can use PEmicro’s USB Multilink Universal FX

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320143&productTab=1

"NOTE: For production usage, see the Cyclone LC and Cyclone FX stand-alone programmer, test & debug interfaces."

You can also look at the list of PE micro products for more details about the available debug probes/ flash programmers, see http://www.pemicro.com/products/product_processor.cfm

 

Best regards,

Diana

0 件の賞賛
返信
3,325件の閲覧回数
ArchieLuo
Contributor III

可以使用Cyclone LC 或者 Cyclone FX,这两个工具是可以脱机烧录的,一般量产都会用这个工具。

U-MULTILINK-FX只是个调试器,必须连电脑使用。

可以使用PROGS12ZZ这个软件,搭配下载器使用。

如有疑问可以联系我~

 

0 件の賞賛
返信
3,283件の閲覧回数
YANG-NMOG
Contributor I

谢谢您的回复!

0 件の賞賛
返信