FOC driving for S12ZVML-MINIBRD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FOC driving for S12ZVML-MINIBRD

1,371件の閲覧回数
87107999
Contributor I

Does S12ZVML-MINIBRD support 3-phase Sensorless Single-Shunt PMSM S12ZVM Application – FOC driving? Or do you have software package for  FOC driving on 

S12ZVML-MINIBRD kit? Thanks

0 件の賞賛
返信
1 返信

1,201件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Xu,

please look at the document  software ported from AN5327 

"The package contains of AN5327_SW ported to S12ZVML-MINIBRD hardware. Just minor changes are introduced, such as removing a button control, moving the LED light to another pin and using internal oscillator."


I hope it help you

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信