S12ZVML-MINIBRD software ported from AN5327

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVML-MINIBRD software ported from AN5327

S12ZVML-MINIBRD software ported from AN5327

The package contains of AN5327_SW ported to S12ZVML-MINIBRD hardware. Just minor changes are introduced, such as removing a button control, moving the LED light to another pin and using internal oscillator.

This is just a working version, it is NOT an official release!!!

AN5327_SW_CW11_MINIBRD.ZIP

CodeWarrior 11.0 and AMMCLib 1.1.13 or higher is required to run this example. If you are not sure about the AMMCLib version, please download the general AN5327_SW from the www.nxp.com/automcdevkits first, install it and then unzip and use the example above.

Labels (1)
Attachments
Comments

The package doesn’t seem to work.

Hi, can you be more specific, please?

No ratings
Version history
Last update:
‎09-13-2018 06:39 AM
Updated by: