FET driver MC33937A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FET driver MC33937A

1,974 次查看
yaletron
Contributor II

Hi,

 

How do I change drive board from 42V to 52V of MTRCKTSBNG128 development kit?  Drive board has FET driver MC33937A.

 

Thanks!

 

John

标签 (1)
2 回复数

1,818 次查看
RadekS
NXP Employee
NXP Employee

Hi john,

MTRCKTSBNG128 contains two boards.

Board with MCU is designed for powering up to 18V (MC33905 is designed for supply voltages up to 28V).

Board with MC33937A FET driver could run up to 58V. You need at least modify voltage dividers. See 3-Phase BLDC/PMSM Low Voltage Power Stage User Manual​ for DC Bus voltage and Back EMF signals voltage dividers.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,818 次查看
yaletron
Contributor II

Thanks Radek,

It was very helpful!

Happy New Year!

John

0 项奖励
回复