FET driver MC33937A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FET driver MC33937A

1,968件の閲覧回数
yaletron
Contributor II

Hi,

 

How do I change drive board from 42V to 52V of MTRCKTSBNG128 development kit?  Drive board has FET driver MC33937A.

 

Thanks!

 

John

ラベル(1)
2 返答(返信)

1,812件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi john,

MTRCKTSBNG128 contains two boards.

Board with MCU is designed for powering up to 18V (MC33905 is designed for supply voltages up to 28V).

Board with MC33937A FET driver could run up to 58V. You need at least modify voltage dividers. See 3-Phase BLDC/PMSM Low Voltage Power Stage User Manual​ for DC Bus voltage and Back EMF signals voltage dividers.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,812件の閲覧回数
yaletron
Contributor II

Thanks Radek,

It was very helpful!

Happy New Year!

John

0 件の賞賛
返信