External memory accessing in XGATE ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External memory accessing in XGATE ?

2,702 次查看
YongJun
Contributor I
Dear.
 
I have some problems in using XGATE to access external memories.
 
I designed TFT Lcd control system through MC9S12XDP512 , and external flash memory is connect to CS0 and lcd contoller to CS1.
 
I hope to transfer image data from external flash memory to lcd controller using
 
XGATE.
 
However , trying to access global address in XGATE Code, the system become halt.
 
// interrupt handler
interrupt void SoftwareTrigger0_Handler(MyDataType* __restrict pData) {
 unsigned long ulAddr;
 
 for(ulAddr=0;ulAddr<0x1000;ulAddr++) {
 *(word *)(0x180000L + (ulong)(ulAddr<<1)) = 0x0000;
 }

 // Clear Software Trigger.
  *(word *)(0x380+0x18) = 0x0100;
}
 
How can I access external memory in XGATE code?
 
 

Message Edited by YongJun on 04-12-200611:52 PM

标签 (1)
0 项奖励
回复
1 回复

743 次查看
Alban
Senior Contributor II

Hello,

On S12XDP family, the XGate has no access to the external addressing space.

Please have a look at the XGate memory map in the device datasheet and it will show you how the 64KB space is attributed.

Cheers,
Alban.

0 项奖励
回复