Does MC9S12 get unique ChipID exist?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MC9S12 get unique ChipID exist?

1,031 Views
everkimage
Contributor IV

I wanna use it to help getting a random number.

Or kindly,someone teach me how to get a random number without using ChipID.

0 Kudos
Reply
2 Replies

921 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

there is a possibility to ensure unique ID to be added during the first MCU start or during flashing the code into the MCU.
There is an IFR field in the MCU with the Program Once Field which can be used for this purpose. However, implementation is up to you.

You can also do it via, for example, sending data via SCI from the PC to the MCU together with processing it as writing unique ID into Program Once field. (The list of used unique IDs could be stored in the PC)

Best regards,

Ladislav

0 Kudos
Reply

921 Views
kef2
Senior Contributor V

Some derivatives like S12P have program once locations, which you could program with unique ID at your production line. Seems like there's no S12 with unique chip ID.

0 Kudos
Reply