Do any NXP MCUs have a -55C low end operating range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do any NXP MCUs have a -55C low end operating range

809件の閲覧回数
larrycarleton
Contributor I

I am an applications engineer for Arrow electronics. Helping a customer who is looking for a MCU with a -55C to 125C operating range. All I can find at the NXP website is MCUs with -40 to 125 or 150C range.

thanks for your support

Larry

ラベル(1)
0 件の賞賛
返信
1 返信

750件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Larry,

Unfortunately, I am not aware of any S12 device qualified for the temperature range from -55°C.

There is one PowerPC MCU with that specification - MPC5554

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/mpc5xxx-5x...

Some of our products are also delivered by e2v Company with such temperature range – from -55°C

http://www.e2v.com/products/semiconductors/processors/

http://www.e2v.com/news/e2v-adds-high-reliability-qorivva-microcontrollers-to-its-portfolio-of-semic...


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信