Difference between MC9S12XEP100MAL and S912XEP100W1MAL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Difference between MC9S12XEP100MAL and S912XEP100W1MAL

跳至解决方案
2,096 次查看
Binsni
Contributor I

Hello,
What is the difference between the MC9S12XEP100MAL and the S912XEP100W1MAL ?
Is it only a different mask set? If yes, can you then tell me what it is?


Regards, Nico

0 项奖励
回复
1 解答
2,088 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

as you can find in the reference manual, chapter ordering info, the device starting with prefix S is automotive specified device with mask set code included in the part number. The device S912XEP100W1MAL contains mask set 1N35H (code W1). The device with the prefix MC is device with any possible mask set. The mas set is presented at the package directly. If you order an MC device then it is not able to order specific mask set.

Each mask set has its own errata list.

Best regards,

Ladislav

在原帖中查看解决方案

2 回复数
2,089 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

as you can find in the reference manual, chapter ordering info, the device starting with prefix S is automotive specified device with mask set code included in the part number. The device S912XEP100W1MAL contains mask set 1N35H (code W1). The device with the prefix MC is device with any possible mask set. The mas set is presented at the package directly. If you order an MC device then it is not able to order specific mask set.

Each mask set has its own errata list.

Best regards,

Ladislav

2,049 次查看
Matttman
Contributor I

What is a mask set?  Is it firmware?  Since these are flash parts, can I use the S912XEP100W1MAL part by erasing the first and then reprogram it?

 

0 项奖励
回复