DP512 Self flash programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DP512 Self flash programming

1,948件の閲覧回数
monstor
Contributor II

I would like to upgrade the flash program of DP512 MCU by CAN bus. Would DP512 has Bootloader to support this function? Can DP512 overwrite its own flash memory?

 

Thank you.

ラベル(1)
0 件の賞賛
返信
1 返信

1,668件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Henry,

Please look at our application note AN2546 HCS12 Load RAM and Execute Bootloader User Guide

http://www.nxp.com/files/microcontrollers/doc/app_note/AN2546.pdf

https://www.nxp.com/webapp/Download?colCode=AN2546SW

Related application note with AN2546 update to S12XE is AN3391 LFAE Bootloader Example and Interface for use with AN2546 (CAN bootloader for S12XE)

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3391.pdf

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3391SW.zip

Other bootloader code which could be used with S12D is AN3275 S12 All-Access Bootloader for the HCS12 Microcontroller Family

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3275.pdf

http://www.nxp.com/webapp/sps/download/license.jsp?colCode=AN3275SW

This bootloader uses just SCI channel to loading code into MCU, CAN interface missing there.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信