DEVKIT-S12G128 PWM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEVKIT-S12G128 PWM

2,525件の閲覧回数
robertwynn
Contributor I

I have a DEVKIT-S12G128, 8Mhz crystal. CodeWarrior 5.9.0. The issue I have is with the PWM. I have setup a 24Mhz bus clock and a 24kHz PWM (16bit) channel (10%duty) . Everything looks ok if you look at a few cycles of the PWM. After about 230ms the output STOPS and restarts in another 230ms.

//---------------------------------

// example devkit-s12g128 with 8MHz crystal
// output on pin PP1 (J2-01)
//
// 24khz pwm signal with a 10% duty cycle.
// After about 230ms the output STOPS. It restarts after about 230ms.
//
// At 1% duty the output stops after 22ms. It restarts after about 440ms

#include <hidef.h>  
#include "derivative.h"

void SetPEEmodeBUSCLK(byte _synr, byte _refdv, byte _postdiv);

void main(void)
{
  ECLKCTL_NECLK = 0;
  DDRP =0x02;
 
  SetPEEmodeBUSCLK(0x02, 0x80, 0x00);   // 24MHz BUSCLK from 8 MHZ oscclk, PEE mode
        
  //------------------------------------------------    
  PWME = 0x00;        // Disable all PWM channels
  PWMPOL =0xFF;       // All channels are high an go low
  PWMCLK = 0x00;      // All channels are clocked from A or B clock source
  PWMCLKAB = 0x00;    // Clock A is the source clock for all channels
  PWMPRCLK = 0x00;    // Clock A & B equal to BUS clock
  PWMCAE = 0x00;      // left aligned
  PWMCTL = 0x10;      // 0-1 concatenated to form 16-bit PWM
 
  PWMPER01 = 1000;    // PWM channel 01 period
  PWME = 0x02;        // Enable the channel
  PWMDTY01 = 100;     // set duty cycle for 01
 
  //-------------------------------------------------
  for(;;)
  {
    _FEED_COP();  
  }
 
}

void SetPEEmodeBUSCLK(byte _synr, byte _refdv, byte _postdiv)
{
 CPMUSYNR    = _synr;
 CPMUREFDIV  = _refdv;
 CPMUPOSTDIV = _postdiv;

 CPMUOSC_OSCE = 1; //enable external oscillator OSCE

 while(!CPMUFLG_UPOSC)
  {// you can check for timeot here with error message report
  };
 while(!CPMUFLG_LOCK)
  {// you can check for timeot here with error message report
  };

  //--- select clocks --------------------
  CPMUCLKS = 0B10000011;                   // bus=fPLL/2; COP is clocked from OSCCLK
  if(CPMUCLKS != 0B10000011)               // After writing CPMUCLKS register, it is strongly recommended to read
  {                                       // back CPMUCLKS register to make sure that write of PLLSEL,
    asm nop;                             // RTIOSCSEL, COPOSCSEL0 and COPOSCSEL1 was successful.
  }
}

0 件の賞賛
返信
4 返答(返信)

2,201件の閲覧回数
robertwynn
Contributor I

Daniel

  I have monitored ECLK it looks fine. The board does not restart.  Here are a few scope plots.

Robert

F0006TEK.JPG

F0005TEK.JPGF0008TEK.JPG

0 件の賞賛
返信

2,201件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

 

Thank you for the plots.

Have you tried running only the code you posted?

The PWM1 function of PP1 has highest priority, so the PWM module controls the pin if enabled.

Unless it is embedded in a project where you could accidently disable the PWM.

Could you halt the program when the PWM is stopped and check all PWM registers?

 

Regards,

Daniel

0 件の賞賛
返信

2,201件の閲覧回数
robertwynn
Contributor I

Daniel

  That is all the code. I have reloaded all the pwm registers in the main loop and that did not work either. I don't know how to halt the code when the PWM is stopped.

One note the code runs if I don't use the PLL. I need the fast/more accurate clock for my project. 

I have mask 0N51A

Robert

0 件の賞賛
返信

2,201件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

I have just run the code on TWR-S12G128 and everything works. It doesn't stop.

Could you monitor BUS clock on ECLK?

Regards,

Daniel 

0 件の賞賛
返信