Codewarrior 10.7 & 11 S12ZVLA12F0MLC project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 10.7 & 11 S12ZVLA12F0MLC project

Jump to solution
2,108 Views
huang_hw
Contributor II

I am trying to create a new barebone project with S12ZVLA12F0MLC (LQFP32, 128k Flash).

The devices under S12Z -> S12ZVL Family has the following devices:

MC9S12ZVL8

MC9S12ZVL16

MC9S12ZVL32

MC9S12ZVL96

MC9S12ZVL128

MC9S12ZVLA64

MC9S12ZVLA96

MC9S12ZVLA128

MC9S12ZVLS16

MC9S12ZVLS32

I chose MC9S12ZVLA128 which I think is the closest to the targeted device and continued with the project creation.

I chose "Processor Expert" under "Rapid Application Development". The project created successfully.

I then went into the "ProcessorExpert.pe" tab and under "Properties", sub-tab "CPU type", the options in the "pull-down" selection  only have MC9S12ZVLA128MLF, MC9S12ZVLA96MLF and MC9S12ZVLA64MLF (seems to all LQFP48 options with old part numbers)

How can I specify my project is using "S12ZVLA12F0MLC (LQFP32, 128k Flash)" when I create a bare-bone project with Processor Expert using Codewarrior 10.7 or 11.0?

0 Kudos
Reply
1 Solution
1,665 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Please have a look at my video I attached.

Hope it helps

Alice

View solution in original post

0 Kudos
Reply
1 Reply
1,666 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Please have a look at my video I attached.

Hope it helps

Alice

0 Kudos
Reply