Codewarrior 10.7 & 11 S12ZVLA12F0MLC project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Codewarrior 10.7 & 11 S12ZVLA12F0MLC project

跳至解决方案
2,075 次查看
huang_hw
Contributor II

I am trying to create a new barebone project with S12ZVLA12F0MLC (LQFP32, 128k Flash).

The devices under S12Z -> S12ZVL Family has the following devices:

MC9S12ZVL8

MC9S12ZVL16

MC9S12ZVL32

MC9S12ZVL96

MC9S12ZVL128

MC9S12ZVLA64

MC9S12ZVLA96

MC9S12ZVLA128

MC9S12ZVLS16

MC9S12ZVLS32

I chose MC9S12ZVLA128 which I think is the closest to the targeted device and continued with the project creation.

I chose "Processor Expert" under "Rapid Application Development". The project created successfully.

I then went into the "ProcessorExpert.pe" tab and under "Properties", sub-tab "CPU type", the options in the "pull-down" selection  only have MC9S12ZVLA128MLF, MC9S12ZVLA96MLF and MC9S12ZVLA64MLF (seems to all LQFP48 options with old part numbers)

How can I specify my project is using "S12ZVLA12F0MLC (LQFP32, 128k Flash)" when I create a bare-bone project with Processor Expert using Codewarrior 10.7 or 11.0?

0 项奖励
回复
1 解答
1,632 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Please have a look at my video I attached.

Hope it helps

Alice

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,633 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Please have a look at my video I attached.

Hope it helps

Alice

0 项奖励
回复