CodeWarrior : MC9S12ZVMAL3V Not supported

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior : MC9S12ZVMAL3V Not supported

Jump to solution
4,424 Views
SLAK
Contributor II

Hi,

 

In order to start dev of a new ECU Project, I am using Codewarrior, but unfortunately the MCU choosed is not supported   "MC9S12ZVMAL3VLF"

Is there anyway to add it to my IDE and also have a SDK + LIN Slave Stack already existing that needs only configuration to fit my project needs?

 

Thanks,

 

 

 

Tags (3)
0 Kudos
Reply
1 Solution
4,382 Views
RadekS
NXP Employee
NXP Employee

Hello SLAK,

It is a bit hard to answer here.

The LIN tack for S12Z isn't production-ready software according to our terminology (SPICE level B at least). On another side, it isn't pure example software.

We have LIN conformance test certificate, provided by a third party (C&S).

So, you may use it in production and expect some quality level, however, it is without a standard quality pack and warranty.
Anyway, many customers are using it in production already.

We have Test pass rate = 100%

Best regards

RadekS

View solution in original post

0 Kudos
Reply
4 Replies
4,416 Views
RadekS
NXP Employee
NXP Employee

Hello SLAK,

The MC9S12ZVMAL3V part number isn't in the system and does not fit with standard nomenclature.

I expect some typo error in the part number.

Are you looking for :

image.png

Did you try to update your installation of the Codewarrior?

 

Unfortunately, we do not offer any SDK for S12Z devices.

The LIN stack is available at https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW-LIN2X-J2602-D

For a fresh start, you may use the Processor Expert tool for code generation and easy prototyping.
Or, you may look at some technical example code S12(X) and S12 MagniV - available Examples and Documents

If you target motor control applications, you may start directly with some motor control kit/board:

 

I hope it helps you.

Best regards

RadekS

 

 

0 Kudos
Reply
4,403 Views
SLAK
Contributor II

Hi Radek,

 

Thanks for your answer.

You are right it was about ZVMAL32.

And thanks for LIN stack link, Is this Stack qualified for a use in serial production projects or it is just for Prototyping ?

 

0 Kudos
Reply
4,383 Views
RadekS
NXP Employee
NXP Employee

Hello SLAK,

It is a bit hard to answer here.

The LIN tack for S12Z isn't production-ready software according to our terminology (SPICE level B at least). On another side, it isn't pure example software.

We have LIN conformance test certificate, provided by a third party (C&S).

So, you may use it in production and expect some quality level, however, it is without a standard quality pack and warranty.
Anyway, many customers are using it in production already.

We have Test pass rate = 100%

Best regards

RadekS

0 Kudos
Reply
4,376 Views
SLAK
Contributor II

Thanks Radek for clear information.

Can you add a link to this conformance test report please?

0 Kudos
Reply