MM9Z1_638 Filter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1_638 Filter

Jump to solution
2,876 Views
Boris_Bloxsberg
Contributor III

Hi,

some weeks ago I added a question regarding the Filter of the MagniV.

Now, I´ve got an additional question....

At page 139 of the manual of the MM9Z1_638  I found the main structure of the implemented low pass filter. In table 192, I found the value conversation: "Data Format: MSB = Sign (“1” minus)"

Does it mean, you are using the twos complement? and is there an excel sheet aviable to calculate new values?

regards.

0 Kudos
Reply
1 Solution
2,863 Views
StanoA
NXP TechSupport
NXP TechSupport

Hi Boris,

It is used the fractional arithmetic in this case so the MSB is sign bit. The number is in range of +-1.000 on 15-bits (14:0).

Attached is the excel sheet for this calculation too.

I hope it could help you in your task.

Best Regards,

Stano.

View solution in original post

1 Reply
2,864 Views
StanoA
NXP TechSupport
NXP TechSupport

Hi Boris,

It is used the fractional arithmetic in this case so the MSB is sign bit. The number is in range of +-1.000 on 15-bits (14:0).

Attached is the excel sheet for this calculation too.

I hope it could help you in your task.

Best Regards,

Stano.