CodeWarrior : MC9S12ZVMAL3V Not supported

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior : MC9S12ZVMAL3V Not supported

跳至解决方案
3,506 次查看
SLAK
Contributor II

Hi,

 

In order to start dev of a new ECU Project, I am using Codewarrior, but unfortunately the MCU choosed is not supported   "MC9S12ZVMAL3VLF"

Is there anyway to add it to my IDE and also have a SDK + LIN Slave Stack already existing that needs only configuration to fit my project needs?

 

Thanks,

 

 

 

标记 (3)
0 项奖励
回复
1 解答
3,464 次查看
RadekS
NXP Employee
NXP Employee

Hello SLAK,

It is a bit hard to answer here.

The LIN tack for S12Z isn't production-ready software according to our terminology (SPICE level B at least). On another side, it isn't pure example software.

We have LIN conformance test certificate, provided by a third party (C&S).

So, you may use it in production and expect some quality level, however, it is without a standard quality pack and warranty.
Anyway, many customers are using it in production already.

We have Test pass rate = 100%

Best regards

RadekS

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,498 次查看
RadekS
NXP Employee
NXP Employee

Hello SLAK,

The MC9S12ZVMAL3V part number isn't in the system and does not fit with standard nomenclature.

I expect some typo error in the part number.

Are you looking for :

image.png

Did you try to update your installation of the Codewarrior?

 

Unfortunately, we do not offer any SDK for S12Z devices.

The LIN stack is available at https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW-LIN2X-J2602-D

For a fresh start, you may use the Processor Expert tool for code generation and easy prototyping.
Or, you may look at some technical example code S12(X) and S12 MagniV - available Examples and Documents

If you target motor control applications, you may start directly with some motor control kit/board:

 

I hope it helps you.

Best regards

RadekS

 

 

0 项奖励
回复
3,485 次查看
SLAK
Contributor II

Hi Radek,

 

Thanks for your answer.

You are right it was about ZVMAL32.

And thanks for LIN stack link, Is this Stack qualified for a use in serial production projects or it is just for Prototyping ?

 

0 项奖励
回复
3,465 次查看
RadekS
NXP Employee
NXP Employee

Hello SLAK,

It is a bit hard to answer here.

The LIN tack for S12Z isn't production-ready software according to our terminology (SPICE level B at least). On another side, it isn't pure example software.

We have LIN conformance test certificate, provided by a third party (C&S).

So, you may use it in production and expect some quality level, however, it is without a standard quality pack and warranty.
Anyway, many customers are using it in production already.

We have Test pass rate = 100%

Best regards

RadekS

0 项奖励
回复
3,458 次查看
SLAK
Contributor II

Thanks Radek for clear information.

Can you add a link to this conformance test report please?

0 项奖励
回复