Code Warrior for 9S12XDP512?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior for 9S12XDP512?

Jump to solution
3,212 Views
roberthiebert
Senior Contributor I

Which version of Code Warrior Special Edition should I be using for use with the 9S12XDP512? Looking at the selections offered I couldn't find one that specified this particular target.

Labels (1)
0 Kudos
Reply
1 Solution
3,059 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome! if you regard this thread is solved, please help us to mark the correct and helpful answer, thanks!

View solution in original post

0 Kudos
Reply
7 Replies
3,059 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
3,059 Views
roberthiebert
Senior Contributor I

Thanks Erich, but when I go here

Special Edition Software

and look at the info on CW12V5.1, the 9S12XDP512 is not on the list of supported microcontrollers, or am I missing it somewhere?

0 Kudos
Reply
3,059 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

i think you should click "i" icon of the item in

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SPECIALEDITIONS

this is the "new feature" of CW5.1, but not all the 5.1 features.

CW5.1 can well support all HC12,HCS12 and HCS12X family chips.

----------------------------------------------------------------------------------------------------------------------------------------------------------

CodeWarrior Development Studio for S12(X) Microcontrollers V5.1 adds the following new features: 

  • Optimization features to improve page management
  • Support for the following microcontrollers:  Support for Open Source BDM connection on S12(X) Tower boards
    • MC9S12G128, MC9S12G96
    • MC9S12GN16, MC9S12GN32
    • MC9S12I128
    • MC9S12XB256
    • MC9S12XHY128, MC9S12XHY256
    • MC9S12XHZ256, MC9S12XHZ384
  • Support for Windows 7 (32-bit and 64-bit platforms)
  • Support for Windows XP and Windows Vista (64-bit platforms)
0 Kudos
Reply
3,059 Views
roberthiebert
Senior Contributor I

I did click the "i" icon but didn't , and still don't see any mention of the 9S12XDP512.

No matter. If you say it will work then that's the answer I was looking for.

Thanks

0 Kudos
Reply
3,059 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

you are correct there is no mention if click i button. it only mentioned the new feature and improvement. all features are listed in its main page: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X&tid=CWH

0 Kudos
Reply
3,059 Views
roberthiebert
Senior Contributor I

Thanks.

0 Kudos
Reply
3,060 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome! if you regard this thread is solved, please help us to mark the correct and helpful answer, thanks!

0 Kudos
Reply